AXIS#.CS.STATE

Description

AXIS#.CS.STATE returns the internal state machine value of the controlled stop.

0 = controlled stop is not occurring.

1 = controlled stop is occurring

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

Fieldbus Information

FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.CS.STATE 0x5002 0x1 USINT - - RO False
AXIS2.CS.STATE 0x5102 0x1 USINT - - RO False

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen